You are here: KAS IDE Reference > Use the Dictionary

Create Variables

Use the Dictionary

For explanations on dictionary usage, including how to create and rename variables, Dictionary Contextual Menu

Create Variables from the Editors

You can create variables directly from the IEC"International Electrotechnical Commission" IEC is a not-for-profit, non-governmental international standards organization that prepares and publishes International Standards for all electrical, electronic and related technologies 61131-3 editors, as follows:

FBD"Function block diagram" A function block diagram describes a function between input variables and output variables. A function is described as a set of elementary blocks editor

  1. Click the dedicated button
    Add Variable in FBD Editor
  2. Figure 4-86: Add Variable in FBD Editor

  3. Click a location in the editor (or double-click the variable if it is already created)
  4. Edit the name in the Variable Editor (or select an existing variable within the list which is already filtered according to their relevant data type)
    Define Variable Name in FBD Editor
  5. Figure 4-87: Define Variable Name in FBD Editor

  6. The KAS IDE"Integrated development environment" An integrated development environment is a type of computer software that assists computer programmers in developing software. IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger automatically checks if the variable already exists. If it is new, you have to:
  7. Define Variable Type in FBD Editor

    Figure 4-88: Define Variable Type in FBD Editor

FBD variables

FFLD editor

  1. Double-click the in or out pins of the function block
    Add a Variable in the FFLD Editor
  2. Figure 4-89: Add a Variable in the FFLD Editor

  3. Edit the name (or select an existing variable within the list which is already filtered according to their relevant data type)
    Define a Variable Name in the FFLD Editor
  4. Figure 4-90: Define a Variable Name in the FFLD Editor

  5. The KAS IDE automatically checks if the variable already exists. If it is new, you have to:
  6. Figure 4-91: Define a Variable Type in the FFLD Editor

Data Types

You can create a variable of available Data Types.

For a list of types, List of Data types

Arrays

Complex Structures

Complex variables are arrays, structures, and instances of function blocks. The following features are allowed for programming:

There is almost no limitation in the amount of complex data declared (theoretically up to 4GB, but practically limited by the memory available in the runtimeIn computer science, runtime (or run-time) describes the operation of a computer program, the duration of its execution, from beginning to termination (compare compile time). Within KAS, runtime also refers to the virtual machine that manage the program written in a computer language while it is running)

For more explanations on the Structure concept, refer to Structures

Declare the structure

  1. Right-click in the Dictionary to open the menu
  2. Select the Add structure command
    Add a Complex Structure
  3. Figure 4-93: Add a Complex Structure

  4. Right-click on the newly created structure and select the Rename structure command
    Rename Complex Structure
  5. Figure 4-94: Rename Complex Structure

  6. Right-click on the new structure and select the Add variable command
    Add Variable to a Complex Structure
  7. Figure 4-95: Add Variable to a Complex Structure

  8. Expand the new structure
  9. Double-click on the new nested variable and define its name and type
  10. Repeat steps 5 and 7 to add all the requested variables

Create an instance of the structure

When finalized, you can drag-and-drop the structure from the library in the (Project) node to a program just like any other function block. A new instance is automatically created.

  1. Select the new structure and move it with a drag-and-drop operation to the program declaration within the Dictionary
    Create an Instance of the Structure
  2. Figure 4-96: Create an Instance of the Structure

  3. You can also add a variable in the Dictionary with the Add variable command. Then double-click on the new variable to define its type by selecting the structure type which is displayed in the Type drop-down menu.
  4. Then you can drag this new instance and drop it in your program like any other variable

Concept Link IconSee Also

 

Use the Dictionary

Create Variables from the Editors

Data Types

Create Complex Structures

Variable Editor

Editing Variables as Text


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™